Prøv at søge efter nøgleord, ordre- eller produktkode eller serienummer, f.eks. “CM442” eller “Teknisk information”
Indtast mindst 2 tegn for at starte søgningen.

Endress+Hauser on further path to growth

Production of level and pressure measurement technology in Maulburg expanded

Endress+Hauser has invested roughly 46 million euros in the expansion of its Maulburg, Germany location. The project, which took nearly two years to complete, includes a new production and office building with more than 17,000 square feet of space, plus a parking garage. The expansion was in response to strong growth in the area of level and pressure measurement technology.

With roughly 2,000 employees, Maulburg is one of the Endress+Hauser Group’s largest locations. “The new buildings will allow us to cope with the growth stemming from previous years,” said Dr Peter Selders, Managing Director of Endress+Hauser Level+Pressure in Maulburg at the dedication of the new facilities. A generous amount of space and a modern infrastructure will help meet the demand for quality and efficiency.

Sustainable building technology

The new multistory building was completed in 2020 and contains 17,000 square feet of space, 11,000 of which is dedicated to production. The design placed considerable value on energy efficiency and features a photovoltaic system on the roof and a cogeneration unit that supplies electricity and heat. Endress+Hauser measurement technology monitors the flow of energy. The Maulburg campus also boasts a new, nearly 17,000-square-foot parking garage with 700 parking spaces.

Highly precise calibration

Still under construction in the basement of the new building are two measurement sections that will be used for the precise calibration of level measurement instruments with radar technology employed in large tanks and silos. At 55 meters each, these measurement sections are the longest of their kind in the world. Customers have a keen interest in calibration given that the smallest measurement deviations can lead to a high degree of uncertainty when monitoring inventories.

Dedication ceremony

The new buildings were officially dedicated in a small gathering on Friday 8 October 2021 in the presence of guests from government and industry, business partners and employees. Although the spaces were occupied in early 2020 after construction was completed, the dedication ceremony was delayed until now due to the coronavirus pandemic.

“Over the past year we shifted a lot of things to the virtual environment, but we wanted to celebrate the opening together with people here in our new building, albeit in a small group due to the Covid restrictions,” emphasized Peter Selders.

As a symbol of sound cooperation, Matthias Altendorf unveiled a mural from German artist Britta Schmidhauser as a gift for the Maulburg location that consists of multicolored rectangles made from fused glass. “If one of the rectangles was missing, the picture would be incomplete,” said the CEO of the Group during the handover of the artwork. “This idea is easily transferred to various Endress+Hauser locations around the world and also applies to all employees.”

New buildings in Maulburg, Germany. ©Endress+Hauser

Endress+Hauser expanded its level and pressure measurement production in Maulburg, Germany.

Inauguration in Maulburg, Germany: Handover of the mural named Global Player. ©Endress+Hauser

Matthias Altendorf hands over a rectangle made of fused glass to Dr Peter Selders in front of the new building, from which the new mural “Global Player” is made.

Dr Peter Selders, Managing Director of Endress+Hauser Level+Pressure in Maulburg. ©Endress+Hauser

Dr Peter Selders, Managing Director of Endress+Hauser Level+Pressure in Maulburg.

Matthias Altendorf, CEO of the Endress+Hauser Group. ©Endress+Hauser

Matthias Altendorf, CEO of the Endress+Hauser Group.

Kontakt