Traditional linear models follow a "take, make, dispose" approach. Circular economy principles seek to retain the value of materials and resources for longer through efficient use, reuse, recovery and closed-loop approaches.
For manufacturers, this requires considering resource use throughout the lifecycle, from raw materials and production to reuse and recovery.
Circular manufacturing starts with understanding how resources move through processes and where value can be retained. More efficient production, longer lifecycles and the reuse of suitable materials and process outputs can help reduce dependence on virgin resources while supporting more resilient operations.
Use resources efficiently: Identify unnecessary material, water and energy losses and improve the efficiency of industrial processes
Extend useful life: Support approaches that keep products, components and assets in productive use for longer.
Recover and recirculate: Return suitable materials, water and process outputs to production or other productive uses.
Circular manufacturing connects processes and value chains
Circularity often extends beyond an individual process or facility. Secondary materials, reusable process outputs and recovered resources can move between processes, sites and organizations.
Closed-loop approaches and collaboration across value chains can create opportunities to retain resource value and reduce demand for additional raw materials. Reliable information about the quality, quantity and characteristics of these resources can support decisions about their potential reuse.
Water reuse
Keep water in circulation
Treating and reusing water can reduce demand for freshwater resources, reduce dependencies and support more resilient industrial water cycles.
Avanceret spildevandsbehandling til genbrug
Væksten inden for genbrug af vand understøttes af innovative, sikre og avancerede behandlingsmetoder, der bliver mere og mere omkostningseffektive.
I forsøget på at bekæmpe vandmangelbekymringer adopterer kommuner og industrier i stigende grad vandgenvindingspraksisser. Teknologiske fremskridt tilbyder grundlaget for sikker og pålidelig spildevandsbehandling.
Direkte og indirekte genbrug af drikkevand er kendt praksis, men det er afgørende, at man forstår de risici, der forbundet dermed, for at kunne beskytte menneskers og miljøets sundhed.
Procesinstrumenter i membranfiltrering spiller en afgørende rolle i at sikre den højeste vandkvalitet. Den driftsmæssige udfordring er at undgå tilsmudsning, tilstopning og beskadigelse af membranerne.
Med globale vandmangelbekymringer er det nødvendigt, at husholdninger og individuelle brgere adopterer levedygtige metoder til reducering af denne essentielle ressource.
Bæredygtige biobrændsler: Skalering med henblik på en effektiv cirkulær økonomi
Læs mere om, hvordan bæredygtige biobrændsler omdanner vedvarende råmaterialer og affaldsstrømme til værdifulde ressourcer og understøtter målene for cirkulær økonomi, reduceret CO2-udledning og ressourceeffektivitet.
Produktion af biogas og biometan fra slam og organisk affald
Fra affald til værdifulde energistrømme: Se, hvordan produktion af biogas og biometan kombinerer udrådning, opgradering og stabil drift for at understøtte en cirkulær ressourceudnyttelse.
Preventing waste and keeping resources in productive use remain central to a circular economy. When waste cannot be avoided or directly reused, effective waste management can help recover remaining material or energy value and manage residual materials responsibly.
Waste management therefore complements circular economy strategies by addressing resources once prevention and direct reuse are no longer possible.
Affaldshåndteringsprocesser og -teknologier, der fremmer forbedringer inden for den cirkulære økonomi
Effektiv affaldshåndtering er afgørende for bæredygtighed, overholdelse af lovgivningen og virksomhedens succes.
Affaldsforbrænding omdanner ikke-genanvendeligt affald til sikker energi
Termisk affaldsbehandling spiller en vigtig rolle inden for moderne affaldshåndtering, da den reducerer affaldsmængden markant, producerer pålidelig vedvarende energi og fjerner forurenende stoffer fra næringsstofkredsløbet.
Measurement brings transparency to circular processes
Circular improvements depend on knowing how resources move through production. Reliable measurement and process data help provide visibility into inputs, outputs and losses and identify where resources can be used more efficiently. This transparency can support manufacturers in:
Identifying resource losses and efficiency opportunities
Monitoring material and resource flows
Optimizing processes for reuse and recovery
Evaluating improvements using reliable operational data
Measurement therefore connects circular economy ambitions with day-to-day industrial operations.
Measurable progress
Turn circular ambitions into measurable progress
Circular economy initiatives become more actionable when resource flows and improvements are transparent. Relevant indicators depend on the process and application and can include resource consumption, material losses, secondary inputs, recovered outputs and water or energy use.
Understand resource flows: Establish transparency around resource inputs, outputs and losses.
Improve resource efficiency: Identify opportunities to reduce consumption, prevent losses and increase reuse or recovery.
Verify progress: Use reliable operational data to understand whether improvements are delivering the intended results.
Building a more circular industrial future
The transition toward a circular economy goes beyond better end-of-life management. It starts with using resources efficiently, preventing unnecessary losses and identifying opportunities to keep materials, water and other resources in productive use.
Reliable measurement, efficient processes and collaboration across value chains can help manufacturers turn circular economy principles into practical improvements and strengthen resource resilience.
FAQ
Everything you need to know about circular economy in process industries and manufacturing
Slutnoter
Looking for more?
Industriekspertise og applikationsviden
Vores industriekspertise og applikationsviden gør os til en værdifuld partner. Kunder fra mange brancher profiterer af vores erfaring med tusindvis af installationer, når de skal have løst deres udfordringer.
Powering a sustainable future
Learn how Endress+Hauser instrumentation leverages the biogas to biomethane upgrading in a sustainable, efficient and safe manner and contributes to renewable power generation.
Vi værner om dine personlige oplysninger
Vi anvender cookies for at forbedre din browseroplevelse, indsamle statistiske oplysninger med henblik på optimering af webstedets funktionalitet og levere skræddersyede annoncer eller indholdselementer.
Hvis du vælger "Accepter alle", giver du dit samtykke til vores brug af cookies.
Yderligere oplysninger fremgår af vores Cookiepolitik .