Title

Prøv at søge efter nøgleord, ordre- eller produktkode eller serienummer, f.eks. “CM442” eller “Teknisk information”
Indtast mindst 2 tegn for at starte søgningen.

From the laboratory to the field with Raman spectroscopy

Evonik's scalable PAT solution – for greater efficiency, safety, and quality in specialty chemicals manufacturing

Industri: Kemi
Process Engineer and Endress+Hauser Raman probe at Evonik

Resumé

In partnership with Endress+Hauser, Evonik has successfully integrated Raman spectroscopy as a powerful process analysis technology (PAT) from the laboratory to pilot plants, right through to production. This technology delivers real-time data, increases efficiency, reduces costs, and improves product quality. Its flexibility, scalability, and safety make it the key to new savings potential in chemical process development. Customers can benefit directly from this acquired expertise to optimize their own development and production processes in a sustainable manner.

The results: Greater efficiency, safety, and quality

16

installed Raman Rxn2 analyzers

50+

measuring points with Raman Rxn probes

Raman spectroscopy from Endress+Hauser has established itself as a key PAT tool at Evonik. It enables significant efficiency gains, cost reductions, and faster market launch of new products.

Results include:

  • End-to-end process analysis from the laboratory to production
  • Real-time measurements possible at several measuring points at the same time
  • Inline measurements replace manual sampling
  • Suitability for pilot plants with low volumes
  • Reliable operation even under difficult conditions (e.g., ATEX zones)
  • Reduction in the time to market
  • Cost reduction through elimination of laboratory evaluations and reduced personnel costs
  • Increased safety
  • Internal acceptance and acquisition of expertise
Photo of Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

"With Raman spectra, you might be able to assign isolated peaks to individual substances in the mixture. This significantly reduces the calibration effort and quickly leads to quantitative results."

Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

The challenge: Find a versatile, real-time lab-to-process solution

Back in 2016, Evonik launched its company-wide “lab to process” strategy with the aim of embedding PAT technologies early on in process development. Evonik was looking for a process analysis technology that would efficiently support the entire development and optimization process while also helping to reduce costs. The goal was to find a solution that not only provides accurate real-time data but is also versatile enough to be used in a wide variety of process environments – from the laboratory to production.

The technology should:

  • be universally applicable for a wide range of chemicals, states of matter and process conditions
  • be flexible and scalable from the R&D lab to large-scale production facilities
  • be quick to integrate in order to shorten development times and reduce time to market
  • improve product quality through continuous inline measurements
  • function reliably even under demanding conditions such as ATEX zones

Our solution: A scalable PAT Endress+Hauser Raman spectroscopy system

Endress+Hauser provided Evonik with a customized solution based on Raman spectroscopy – a technology that meets all of the requirements outlined. The systems are characterized by their exceptional modularity and versatility. Thanks to optical fibers and various probe types, they can be easily integrated into a wide variety of installation situations. Up to four independent channels enable simultaneous monitoring of multiple measuring points – a clear advantage for complex processes.

The chemometric suitability of the spectra offers particular added value – due to compatibility with all common chemometric programs, these can be analyzed directly on the spectrometer in a way that is versatile, intuitive, and achieved in real time. This allows qualitative and quantitative data to be recorded and interpreted immediately during the process – without any time-consuming manual sampling.

Raman spectroscopy was successfully used for the first time in a pilot plant for the development of hydrogenation processes. The probe was integrated into a 6 mm pipe – significantly smaller than in production facilities. Instead of daily NMR sampling, the technology now enables inline measurements to be taken every single minute, and the process continuously monitored.

This process is efficient, precise, and safe. In pilot plants with low volumes in particular, the system composition remains unchanged because no samples need to be taken. This not only saves time and money but also increases safety for both personnel and plant.

Hazardous area use

Thanks to its standardized and certified components, the Raman system can even be used in ATEX zones at a cost that is reasonable. For use in potentially explosive atmospheres, Evonik also uses the Liquiphant Vibronic level switch. This ensures that no flammable gas mixture can form in the laser beam of the Raman probe – a decisive contribution to process safety.

Testimonial

Photo of Dr. Roland Peschke, PAT expert at specialty chemical manufacturer Evonik

“The requirements for PAT measurement systems are particularly high, especially in the harsh environment of process plants and the need to comply with ATEX regulations. Raman spectroscopy has established itself as a robust and reliable tool in this area.” - Dr. Roland Peschke, PAT expert at Evonik Oxeno

Global roll out

This system has enabled Evonik not only to increase efficiency and quality in process development, but also to successfully transfer technology from the laboratory to production – a real key to new savings potential. Following successful implementation in Germany, Raman technology is now being rolled out internationally in Evonik’s first production plants – supported by the global expertise of Endress+Hauser.

Free download

Download the case study

Want access to the full case study as a PDF? Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the case study

Kontakt os

Er du interesseret i vores løsninger? Skal vi tage en snak om din applikation?

Anmod om mere information

For at anmode om flere oplysninger, bedes du venligst udfylde formularen nedenfor.

Angiv venligst så mange oplysninger som muligt, så vi kan hjælpe dig bedst muligt.

Products and services used

/

Related solutions and technology

Optical analysis

Optical analysis systems for monitoring composition and concentration in solids, liquids, slurries, particles, and gases - for laboratory, process, and emission monitoring.

Yderligere information

Overvågning af spildevandsudledning 

Sørg for, at spildevandsudledningen overholder lovkravene, med komplet og pålidelig overvågning, kontinuerlige måleværdier og hurtig reaktion på forurening.

Læs mere

Måling af brint i naturgasrørledninger

Hurtig, kontinuerlig måling af brint i naturgasrørledninger muliggør sikker iblanding, overholdelse af kvalitetskrav og dynamisk styring ved hjælp af Raman-spektroskopi – uden forbrugsstoffer eller afbrænding

Læs mere

Analyse af biometankvaliteten med henblik på sikker tilførsel til gasnettet og overholdelse af gældende krav 

Opnå en pålidelig biometankvalitet med hurtig og nøjagtig onlinemåling af H₂S, vanddugpunkt og kritiske parametre med henblik på sikker tilførsel til gasnettet og effektiv drift. 

Læs mere

Beskyt RO-membraner med onlineovervågning af vandkvaliteten ved afsaltning 

Pålidelig onlineovervågning af vandkvaliteten beskytter RO-membraner (omvendt osmose), reducerer behovet for rengøring og forlænger membranernes levetid ved afsaltning og genbrug af vand

Læs mere

Detektion af lækager i kryogene tanke (LNG, ethylen, LPG og ammoniak)

Detektér kryogene tanklækager tidligt, og bevar kontrollen. Endress+Hauser leverer kontinuerlig og yderst pålidelig temperaturovervågning for at beskytte mennesker, aktiver og kritisk infrastruktur.

Læs mere

Måling og verifikation af CCUS i realtid

Lås op for fremtiden inden for kulstofopsamling: præcis, pålidelig og skræddersyet til anvendelser i tæt fase

Læs mere

Løsninger til kontinuerlig overvågning af emissioner for at sikre overholdelse af lovgivningen

Løsninger til kontinuerlig overvågning af emissioner for at sikre overholdelse af lovgivningen

Yderligere information

FAQs

Firmalogo af: Evonik Industries AG

Evonik Industries AG, med hovedkontor i Essen, Tyskland, er en af verdens førende virksomheder inden for specialkemikalier. Takket være sin passion for innovation og teknisk ekspertise går virksomheden ud over den traditionelle kemi for at skabe bæredygtige løsninger til industrien og samfundet. Evonik driver produktionsanlæg i 27 lande på seks kontinenter.